TJA1103

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
2,868 Views
Chenxu1
Contributor II


TJA1103
INT_N pin, when there is a trigger event, this pin is temporarily pulled down (for example, pull down 2ms)? Or keep pulling the lower till MCU to handle it?

0 Kudos
Reply
1 Solution
2,854 Views
guoweisun
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
4 Replies
2,862 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

The INT_N pin is driven low when at least one interrupt request (IRQ) is active and enabled. Otherwise, the INT_N pin is high-Z.

0 Kudos
Reply
2,857 Views
Chenxu1
Contributor II
I know.
But, is INT_N pin driven low for several ms, or it stay pulled down and wait for the MCU to process it?
0 Kudos
Reply
2,855 Views
guoweisun
NXP TechSupport
NXP TechSupport

Keep low always.

0 Kudos
Reply
2,848 Views
Chenxu1
Contributor II

OK,Thanks

0 Kudos
Reply