TJA1103

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,889件の閲覧回数
Chenxu1
Contributor II


TJA1103
INT_N pin, when there is a trigger event, this pin is temporarily pulled down (for example, pull down 2ms)? Or keep pulling the lower till MCU to handle it?

0 件の賞賛
返信
1 解決策
2,875件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
4 返答(返信)
2,883件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

The INT_N pin is driven low when at least one interrupt request (IRQ) is active and enabled. Otherwise, the INT_N pin is high-Z.

0 件の賞賛
返信
2,878件の閲覧回数
Chenxu1
Contributor II
I know.
But, is INT_N pin driven low for several ms, or it stay pulled down and wait for the MCU to process it?
0 件の賞賛
返信
2,876件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Keep low always.

0 件の賞賛
返信
2,869件の閲覧回数
Chenxu1
Contributor II

OK,Thanks

0 件の賞賛
返信