TEA2096 application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA2096 application

4,332 Views
arunava_paul
Contributor II

Hi. I need to implement synchronous rectification in my 150W push pull converter secondary side. I have choosen TEA2096 for that. The secondary side has two diodes as shown in the figure and I am planning to replace them with mosfets that will be driven through a single IC chip. What are the challenges I might face while trying to implement that? output is 5V and output current demand is around 20Amps. And finally, Can I achieve >90% efficiency in the converter with that?

0 Kudos
Reply
5 Replies

4,306 Views
RafaR
NXP Employee
NXP Employee

Hello Paul

Please check the link below

https://www.nxp.com/docs/en/data-sheet/TEA2096T.pdf

Here you can find useful information such as the description of operation with the use of MOSFET with the TEA2096

RafaR_0-1730139894685.png

 

I recommend reading chapters 8 to 13, these chapters have functional description, images, limit values, etc.

Have a great day and best of luck

0 Kudos
Reply

4,301 Views
arunava_paul
Contributor II

Hi RafaR,

Thanks for the input. Is there any spice model of the IC? Can you share me the link? I want to run my model in LTSPICE.

0 Kudos
Reply

4,296 Views
RafaR
NXP Employee
NXP Employee

Hello Paul

Sorry, we do not have a spice model to simulate the TEA2096, we only have the CAD model.

Have a great day and best of luck

0 Kudos
Reply

4,291 Views
arunava_paul
Contributor II

Hi RafaR,

Sorry to hear about that. Can you please atleast confirm that if this IC be utilized for push-pull application. or can you suggest some similiar IC specifically designed for push-pull application?

0 Kudos
Reply

4,272 Views
RafaR
NXP Employee
NXP Employee

Hi Paul

I do not have a document to confirm the application or recommendations of TEA2096 as push-pull but in my opinion do it, I believe it will work, hope it helped you.

Have a great day and best of luck

0 Kudos
Reply