TEA2017DB1580 tune

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA2017DB1580 tune

1,456 Views
Arjun_Bansal
Contributor II

This is a 12v/20amp supply, but i want to tune it to 24v/10amp or 48v/5amp. i want to know if it possible to tune it. Kindly provide feedback on this, looking for urgent response. TEA2017DB1580 TEA6017AT 

Tags (1)
0 Kudos
Reply
1 Reply

1,447 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Arjun,

The TEA2017DB1580, based on the TEA2017 LLC and PFC combo controller, is indeed primarily designed for a 12V/20A output as set by its external components and design configuration. To change the output to 24V/10A or 48V/5A, you would need to make substantial modifications to the feedback loop, transformer winding ratio and possibly the power stage components to support these new voltage and current specifications. Given the complexity of these changes and considering thorough testing that would be essential to ensure stability, efficiency etc. we do not really recommend it.

BRs, Tomas

,