TEA2017DB1580 tune

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TEA2017DB1580 tune

1,465件の閲覧回数
Arjun_Bansal
Contributor II

This is a 12v/20amp supply, but i want to tune it to 24v/10amp or 48v/5amp. i want to know if it possible to tune it. Kindly provide feedback on this, looking for urgent response. TEA2017DB1580 TEA6017AT 

タグ(1)
0 件の賞賛
返信
1 返信

1,456件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Arjun,

The TEA2017DB1580, based on the TEA2017 LLC and PFC combo controller, is indeed primarily designed for a 12V/20A output as set by its external components and design configuration. To change the output to 24V/10A or 48V/5A, you would need to make substantial modifications to the feedback loop, transformer winding ratio and possibly the power stage components to support these new voltage and current specifications. Given the complexity of these changes and considering thorough testing that would be essential to ensure stability, efficiency etc. we do not really recommend it.

BRs, Tomas

,