TEA19161

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA19161

1,885 Views
shouyumi
Contributor I

TEA19161T能否在不与TEA19162合作的情况下实现直接的DC-DC转换?

0 Kudos
Reply
4 Replies

1,863 Views
shouyumi
Contributor I

那我能问一下能不能实现呢?我只想通过TEA19161了解 LLC 电路的工作状态。如果可能的话,你能提供电路图吗?

0 Kudos
Reply

1,874 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The TEA19161 is not designed to achieve direct DC-DC conversion without the TEA19162. They are intended to work together to provide a complete and efficient power conversion solution.

We also do not recommend using the TEA19161 with another PFC controller. The TEA19162 is designed to operate in close cooperation with the TEA19161 to ensure optimal burst-mode operation and complementary protection functions.

BR, Tomas

0 Kudos
Reply

1,859 Views
shouyumi
Contributor I
Thank you very much !
0 Kudos
Reply

1,862 Views
shouyumi
Contributor I
Then may I ask if it can be achieved? I just want to learn about the working state of the LLC circuit through TEA19161. If it is possible, could you provide the circuit diagram
0 Kudos
Reply