Single Phase AC Induction Motor Control Reference Design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single Phase AC Induction Motor Control Reference Design

1,384 Views
Lorenzo_Ziliotto
Contributor I

Hi to everybody,

I'm using the circuit suggest by the Motorola application note DRM039 (circuit of page 23); everything works fine but during the product certification I found that the 2KV surge disturb destroys the circuit!! 

Transil diodes D11 and D18 aren't able to protect the IGBTs. Also a varistor S10K300 at the AC line input is not sufficient to stop the surge transient. I tried to use strong IGBTs (IXYH8N250CHV) without positive results. The load is a 45W fan motor.

Anybody use that circuit? Suggestions to solve my problem?

Thanks a lot.

0 Kudos
Reply
0 Replies