Simple Resonant Inverter, 100 kHz, 100W

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Simple Resonant Inverter, 100 kHz, 100W

2,135 次查看
johnyradio
Contributor II

I need to make a Resonant Inverter, with AC output.

  • Application is an AC power supply
  • Topology: LLC or other
  • Input: 12V to 24V DC
  • No DC output
  • 100 kHz
  • 100W
  • 0 to 20A continuous
  • constant voltage
  • 0 to 5V
  • Inductive load for galvanic isolation
  • pure sine
  • soft-switched
  • 1/2 bridge or 1/4 bridge

Our load uses AC directly from the secondary of the load-trafo. We will not rectify or filter the secondaries of those load-inductors. 

What NXP parts are recommended? Seeking FET's, gate driver, controller, etc

0 项奖励
回复
3 回复数

2,124 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear John,

inverter concept please check this link. You can find there a block diagram with recommended components. We do not have any FETs in our portfolio. For the recommended Gate Drivers, IGBTs or SIC FETs are recommended. 

JozefKozon_0-1684495489210.png

Please also check this link for EV Power Inverter Control Reference Platform Gen 2. 

With Best Regards,

Jozef

 

2,108 次查看
johnyradio
Contributor II

Hello,
Thank you for your recommendations!

But there are some issues:

- Those are heavy-duty EV devices. Ours is a mobile consumer device, so our form factor is small and light.

- Our power requirements are significantly lower. 

- We don't need DC output or rectification. Our load uses AC directly from the secondary of the load-trafo. We will not rectify or filter the secondary. 


Any ideas?
Thx!

0 项奖励
回复

2,051 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello John,

unfortunately we do not have any other inverters in our portfolio. Only the three heavy duty for automotive applications. GD31xx. 

I apologize for inconvenience.

With Best Regards,

Jozef

0 项奖励
回复