Simple Resonant Inverter, 100 kHz, 100W

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple Resonant Inverter, 100 kHz, 100W

2,134 Views
johnyradio
Contributor II

I need to make a Resonant Inverter, with AC output.

  • Application is an AC power supply
  • Topology: LLC or other
  • Input: 12V to 24V DC
  • No DC output
  • 100 kHz
  • 100W
  • 0 to 20A continuous
  • constant voltage
  • 0 to 5V
  • Inductive load for galvanic isolation
  • pure sine
  • soft-switched
  • 1/2 bridge or 1/4 bridge

Our load uses AC directly from the secondary of the load-trafo. We will not rectify or filter the secondaries of those load-inductors. 

What NXP parts are recommended? Seeking FET's, gate driver, controller, etc

0 Kudos
Reply
3 Replies

2,123 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear John,

inverter concept please check this link. You can find there a block diagram with recommended components. We do not have any FETs in our portfolio. For the recommended Gate Drivers, IGBTs or SIC FETs are recommended. 

JozefKozon_0-1684495489210.png

Please also check this link for EV Power Inverter Control Reference Platform Gen 2. 

With Best Regards,

Jozef

 

2,107 Views
johnyradio
Contributor II

Hello,
Thank you for your recommendations!

But there are some issues:

- Those are heavy-duty EV devices. Ours is a mobile consumer device, so our form factor is small and light.

- Our power requirements are significantly lower. 

- We don't need DC output or rectification. Our load uses AC directly from the secondary of the load-trafo. We will not rectify or filter the secondary. 


Any ideas?
Thx!

0 Kudos
Reply

2,050 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello John,

unfortunately we do not have any other inverters in our portfolio. Only the three heavy duty for automotive applications. GD31xx. 

I apologize for inconvenience.

With Best Regards,

Jozef

0 Kudos
Reply