SBC_FS23 API :Sbc_fs23_SetWakeupConfig

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SBC_FS23 API :Sbc_fs23_SetWakeupConfig

ソリューションへジャンプ
2,701件の閲覧回数
WeiC
Contributor I

In the " CDD_Sbc_fs23.c" file ,API "Sbc_fs23_SetWakeupConfig" has two lines code,as follows

/*--------------------------------------------------*/

u16TxData = (u16RxData & (~(SBC_FS23_M_WK1_WUEN_WAKEUP_MASK | SBC_FS23_M_WK2_WUEN_WAKEUP_MASK | SBC_FS23_M_HVIO1_WUEN_WAKEUP_MASK | SBC_FS23_M_HVIO2_WUEN_WAKEUP_MASK | SBC_FS23_M_LVIO3_WUEN_WAKEUP_MASK | SBC_FS23_M_LVIO4_WUEN_WAKEUP_MASK | SBC_FS23_M_LVI5_WUEN_WAKEUP_MASK))) | (*Sbc_fs23_pConfigPtr->Sbc_fs23_WuConfig)[WakeupSettingId].IoWuEnReg;

..................................

u16TxData = (u16RxData & (~(SBC_FS23_M_CAN_WUEN_WAKEUP_MASK | SBC_FS23_M_LIN_WUEN_WAKEUP_MASK | SBC_FS23_M_LDT_WUEN_WAKEUP_MASK))) | (*Sbc_fs23_pConfigPtr->Sbc_fs23_WuConfig)[WakeupSettingId].Wu1EnReg;

/*--------------------------------------------------*/

what means about “(u16RxData & (~............))| XxxxCfg.XxxxEnReg"? why not directly use“(u16RxData | XxxxCfg.XxxxEnReg"?

I don't understand the operation of "u16RxData & (~............)".

 

0 件の賞賛
返信
1 解決策
2,641件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

By using & (~(………)) we make sure that those configurable wake-up and interrupt enable bits are first zeroed before writing a new value to them.  

BR, Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,487件の閲覧回数
nirmal_masilamani
Contributor V

Hi,

I am using SBC FS23, and I am trying to configure it to CAN Wakeup. But SBC wakeup from LPOFF, with all CAN message.

How to configure it for wake up from particular CAN message? Is there a option available in SBC FS23?

 

0 件の賞賛
返信
2,642件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

By using & (~(………)) we make sure that those configurable wake-up and interrupt enable bits are first zeroed before writing a new value to them.  

BR, Tomas

0 件の賞賛
返信