Reserve Power Circuit for LS1012A Design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reserve Power Circuit for LS1012A Design

Jump to solution
3,391 Views
joe1652
Contributor IV

Hello, I am designing a small board with the LS1012A ARM Processor. The board will likely consume about 16W of power. I will need to design a reserve power circuit to supply power to the board for a short amount of time. Does NXP have any devices that I could use to monitor the input power and switch over to some supercaps to provide a short time of power to the board, say 2 seconds or so, enough time for the Processor to finish what it was doing and go through the power down sequence of the Linux OS.

Thanks,

Joe

1 Solution
3,249 Views
joe1652
Contributor IV

 Jose,

Hello, thank you very much for responding to my post. This is very helpful.

Have a great day,

Joe

View solution in original post

4 Replies
3,249 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Joe,

The LS1012A by itself have a 1W typical power dissipation, unfortunately I do not have access to the total power consumption of the LS1012ARDB-PB Development board, but you can enter a new community thread in the QorIQ community to ask this question, you can find this community in the following link: https://community.nxp.com/community/qoriq?tid=community


Have a great day,
Jose

3,249 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Joe,

 

There is a reference design board for the QorIQ LS1012A using the VR5100 as the power management IC I charge of powering the system according to the LS1012A requirements, you can find details of the reference design in the reference manual that you can download from the following link: https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources...

 

Plus, you can find the schematic and board design files by downloading the LS1012ARDB-PB Design files (REV D) on the following link: https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources...

 

The VR5100 have an integrated circuit used as battery backup:

From the On mode, when the voltage at VIN drops below the undervoltage falling threshold, UVDET, the state machine transitions to the Coin Cell mode.

The LICELL pin provides for a connection of a coin cell backup battery or a “super” capacitor. If the voltage at VIN goes below the VIN threshold (VTL1), contact-bounced, or removed, the coin cell maintained logic is powered by the voltage applied to LICELL.

Check the VR5100 datasheet for more details: https://www.nxp.com/docs/en/data-sheet/VR5100.pdf


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,249 Views
joe1652
Contributor IV

Hello, do you know the power consumption for the LS1012ARDB-PB Development board? I find it very exciting that it use Power Over Ethernet. 

Joe

0 Kudos
Reply
3,250 Views
joe1652
Contributor IV

 Jose,

Hello, thank you very much for responding to my post. This is very helpful.

Have a great day,

Joe