Replace mosfet RFPower

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Replace mosfet RFPower

1,776 次查看
thanhphatlk1995
Contributor I

I have RF power. It have 8 kit module use Mosfet MRFE6VP61K25H inside. But only one have been damaged. Now, Mosfet MRFE6VP61K25H unavailable in your store. Could i use new version MRFE6VP61K25HR6 to replace for MRFE6VP61K25H? I need to replace only one mosfet damaged or all to MRFE6VP61K25HR6?
I'm looking forward your feedback soon.

Thanks you for your support.

标记 (1)
0 项奖励
回复
1 回复

1,720 次查看
LPP
NXP Employee
NXP Employee

Yes, you can do it.

R5 or R6 are reel pack ship options.  Devices are exactly the same MRFE6VP61K25H


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复