Regarding USBPHYLDO of PF1510

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding USBPHYLDO of PF1510

Jump to solution
2,803 Views
tomohisa_sakamo
Senior Contributor III

Dear Support-team,

We have below questions about USBPHYLDO of PF1510.
Please support us.

<Question 1>
USBPHY (default 3.3 V output) seems to be described as being enable / disable with USBPHYLDO bit,
In the datasheet, USBPHYLDO = '0' for both Enable and Disable.
*The datasheet  of PF 1550 is also the same description.

Is Enable / Disable control possible? (Is it a typo)?

<Question 2>
If it is set to Disable, will the USBPHY output become 0 V?

Best Regards,
T.Sakamoto@Ryosan

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,657 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Tomohisa,

 

[Answer 1]

This is a typo, USBPHYLDO = ‘0’ is for Disabled and  USBPHYLDO = ‘1’ should be for Enabled.

I reported this typo to the Apps team, I’ll be fixed for the next revision of the datasheet.

 

[Answer 2]

Correct, USBPHY LDO regulator can be 0V if USBPHYLDO bit is disabled (‘0’).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,657 Views
tomohisa_sakamo
Senior Contributor III

Dear Jose-san,

Thank you for your reply.

We understood your answers.

Thank you!

Best Regards,

T.Sakamoto@Ryosan

0 Kudos
Reply
2,658 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Tomohisa,

 

[Answer 1]

This is a typo, USBPHYLDO = ‘0’ is for Disabled and  USBPHYLDO = ‘1’ should be for Enabled.

I reported this typo to the Apps team, I’ll be fixed for the next revision of the datasheet.

 

[Answer 2]

Correct, USBPHY LDO regulator can be 0V if USBPHYLDO bit is disabled (‘0’).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply