RD33771-48VEVM Max Load Current?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RD33771-48VEVM Max Load Current?

1,446 Views
Choist
Contributor I

Hello I purchased and am using RD33771-48VEVM.

The load motor we are currently using is of the high current (70-100[A]) class, so I would like to know how far it can be used.

I want to know what the maximum load current is.

Thank you

#RD33771

#BMS

0 Kudos
Reply
2 Replies

1,406 Views
guoweisun
NXP TechSupport
NXP TechSupport

This BMS part use the shunt resistor 100uΩ which can support test −1500 A to
1500 A (the actual range is in terms of voltage and is given by min and max of VIND) with
a 6.0 mA resolution.

0 Kudos
Reply

1,402 Views
Choist
Contributor I

So, is this model capable of using a motor load of up to +-1500[A]?

I'm afraid the cable might burn out.

0 Kudos
Reply