RD33771-48VEVM Max Load Current?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RD33771-48VEVM Max Load Current?

1,444 次查看
Choist
Contributor I

Hello I purchased and am using RD33771-48VEVM.

The load motor we are currently using is of the high current (70-100[A]) class, so I would like to know how far it can be used.

I want to know what the maximum load current is.

Thank you

#RD33771

#BMS

0 项奖励
回复
2 回复数

1,404 次查看
guoweisun
NXP TechSupport
NXP TechSupport

This BMS part use the shunt resistor 100uΩ which can support test −1500 A to
1500 A (the actual range is in terms of voltage and is given by min and max of VIND) with
a 6.0 mA resolution.

0 项奖励
回复

1,400 次查看
Choist
Contributor I

So, is this model capable of using a motor load of up to +-1500[A]?

I'm afraid the cable might burn out.

0 项奖励
回复