Question on Failing MC33879

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question on Failing MC33879

ソリューションへジャンプ
2,495件の閲覧回数
dkark
Contributor I

Have there been any issues with bad lots of MC33879 Octal Hi/Low Driver Chips? I have one date code that seems to be failing at a high level. Are there resources to check these date codes or see if maybe they are counterfeit chips?

Alternatively from a design perspective, is there any problems running with Vdd (logic 5V) powered and Vpwr (pwr 24V) unpowered for long periods of time? I could not see anything in the data sheets to say this would be an issues. I doubt this is the issue, because all the failed chips have the same date code, and others outside the date code have not been an issue.

タグ(1)
1 解決策
2,443件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

No problem application about VDD power up then unpower Vpwr.

Suggest you do FA about your issue deivce from your purchase channel.

元の投稿で解決策を見る

2 返答(返信)
2,444件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

No problem application about VDD power up then unpower Vpwr.

Suggest you do FA about your issue deivce from your purchase channel.

2,443件の閲覧回数
dkark
Contributor I

Thank you very much for the confirmation about VDD and VPWR. I will follow up with the supplier.

0 件の賞賛
返信