QI - Wireless Power receiver MWPR1516

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QI - Wireless Power receiver MWPR1516

ソリューションへジャンプ
2,634件の閲覧回数
olivier_ctm
Contributor I

Hello,

I already designed the transmitter part of my wireless charger but i have some questions about the MWPR1516 wireless charging IC wich is the NXP component for the receiver part..

First, is it the only receiver available from NXP ? I didn't find others.

Second, what is efficiency of this device ? There are no courbs (efficiency vs output load for some Vout).

Many thanks for your help.

Best regards

 

Olivier

0 件の賞賛
返信
1 解決策
2,622件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Olivier,

yes, the WPR1516 is our only one wireless charging receiver IC. Please refer to this link

Unfortunately we do not have the separate efficiency values for the WPR1516. Generally it is possible to achieve efficiency of the whole system above 60%. Please see the table below. The WPR1500-LDO EVB contains the WPR1516 IC.

JozefKozon_0-1676289927663.pngJozefKozon_0-1676289927663.png

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,623件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Olivier,

yes, the WPR1516 is our only one wireless charging receiver IC. Please refer to this link

Unfortunately we do not have the separate efficiency values for the WPR1516. Generally it is possible to achieve efficiency of the whole system above 60%. Please see the table below. The WPR1500-LDO EVB contains the WPR1516 IC.

JozefKozon_0-1676289927663.pngJozefKozon_0-1676289927663.png

With Best Regards,

Jozef

0 件の賞賛
返信