Programming issue with FlexGUI-PF8X PF8200

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming issue with FlexGUI-PF8X PF8200

Jump to solution
7,265 Views
jack_huang1
Contributor IV

Dear;

        When I use the FlexGUI-PF8X offline tool to program the firmware (SC33PF8200KKES) for the PF8200, the following issue is reported:
        Script parsing failed (wrong format). See Figure 1 for specific information.

       I can burn and write normally using PF8100.

        Thank you!

          Best Regards!

0 Kudos
Reply
1 Solution
7,122 Views
jack_huang1
Contributor IV

Dear;

         谢谢您的支持,已经搞定了,谢谢!

 

 

         Best Regards!

View solution in original post

0 Kudos
Reply
12 Replies
7,250 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi Jack

请问您的script是如何生成的?通过什么方式?还是说直接哪里下载的?

0 Kudos
Reply
7,243 Views
jack_huang1
Contributor IV

Dear;

        该次烧写的固件是直接NXP官网下载的,谢谢!

 

 

      Best Regards!

0 Kudos
Reply
7,242 Views
guoweisun
NXP TechSupport
NXP TechSupport

能发我看看是哪个script吗?

0 Kudos
Reply
7,237 Views
jack_huang1
Contributor IV

Dear;

        固件见附件。谢谢!

 

 

        Best Regards!

0 Kudos
Reply
7,229 Views
guoweisun
NXP TechSupport
NXP TechSupport

我没测试OTP 的script我测试了TBB script是可以运行的,在GUI 选择TBB 以后

我用的是10.0.0的GUI 版本

guoweisun_1-1765352938071.png

 

 

0 Kudos
Reply
7,234 Views
guoweisun
NXP TechSupport
NXP TechSupport

TBB 的那个script能运行吗?

不行的话现在最新的GUI!

GUI PMIC Software | Automotive | NXP Semiconductors

0 Kudos
Reply
7,153 Views
jack_huang1
Contributor IV

Dear;

        我安装了最新的GUI10.0.0版本,但是进去之后,START一致显示是灰色的,我重新更新KL25Z firmware。请问:这个还需要安装什么?谢谢!

 

 

         Best Regards!

0 Kudos
Reply
7,150 Views
guoweisun
NXP TechSupport
NXP TechSupport

看这个附件的文档里面有更新的FW,从第12页开始看4 Installing and configuring software and tools 。

0 Kudos
Reply
7,137 Views
jack_huang1
Contributor IV

Dear;

         我现在使用的是windows 11操作系统,我看这个软件支持的操作系统是windows 10或windows 7,这个是否会影响GUI的正常工作?谢谢!

 

          Best Regards!

 

 

 

Tags (1)
0 Kudos
Reply
7,123 Views
jack_huang1
Contributor IV

Dear;

         谢谢您的支持,已经搞定了,谢谢!

 

 

         Best Regards!

0 Kudos
Reply
7,135 Views
guoweisun
NXP TechSupport
NXP TechSupport

不会,我也是WIN11

0 Kudos
Reply
7,230 Views
jack_huang1
Contributor IV

Dear;

         好的,我按照最新的GUI后测试一下。谢谢!

 

 

        Best Regards!

0 Kudos
Reply