Programmable voltage regulator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programmable voltage regulator

1,135件の閲覧回数
karmegancjk
Contributor III

Hello, in the NXP product, I'm finding a programmable voltage regulator IC with an adjustable voltage of 0–5V for I2C, SPI, or UART interface. I was unable to locate this kind of IC. Voltage resolution +/- 1 mV and output <= 200 mA are the specifications. Could you recommend this specification IC ?

0 件の賞賛
返信
1 返信

1,120件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Karmegancjk,

NXP currently does not offer such a programmable voltage regulator IC. 

Our strategy is to provide highly integrated ICs such as PMICs and SBCs including several buck-boost regulators/LDOs + functional safety features meeting safety integrity levels up to ASIL D, but not standalone programmable LDOs or switching regulators.

You may have already done this, but I would recommend contacting other manufacturers such MaxLinear, ON Semiconductor, Microchip etc.

BRs, Tomas

 

0 件の賞賛
返信