Power dissipation on MC33882

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power dissipation on MC33882

Jump to solution
3,454 Views
ondrej_brejla
Contributor I

Hi,

is there any estimate as to how much power does the MC33882 consume? I'm controlling the outputs through the SPI interface and I'm using just 4 of the high power outputs (LED outputs are also unused). I' m trying to figure out what power DC/DC convertor I need to use to isolate the supply in a project.

Best regards,

Ondrej

0 Kudos
Reply
1 Solution
3,354 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Ondrej,

 

According to the device specification on page 3, VPWR Supply current is max 7.5mA, so make sure you select your DC/DC converter according to this specification.

Unfortunately, there is no further detailed information about the consumption of the MC33882.  


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,355 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Ondrej,

 

According to the device specification on page 3, VPWR Supply current is max 7.5mA, so make sure you select your DC/DC converter according to this specification.

Unfortunately, there is no further detailed information about the consumption of the MC33882.  


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply