Pca9451 single phase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pca9451 single phase

3,696件の閲覧回数
Michaelscott237
Contributor I

Hey, has any one tried using the pca9451 buck 1 and 3 as single phase?

The evb doesn't seem to work for using that configuration so i thought maybe trying to design my own board with that device using buck 1,3 as single phase but i dont see any documentation for that.

Has anyone tried that and it worked?

If so, can you post a reference for that? 

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

3,670件の閲覧回数
Michaelscott237
Contributor I

Hey, thanks for the reply. 

I did exactly as you shown and i get 0.903 on buck 1 and 0.896 on buck3.

Did you tried using forced pwm mode on buck 3?

That what caused the problem for me before, and i don't want to try that again on a new board

0 件の賞賛
返信

3,689件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Michael,

I have just tested my PCA9451A-EVK for BUCK1 and BUCK3 single phase and it works correctly. Please make sure to follow the steps in the section 3. in the Getting Started with PCA9451A-EVK when turning on the EVB. Set the J30 to 2-3 position and remove jumper from the J36 (open). 

JozefKozon_0-1736926175546.png

Then please try the following configuration in the GUI. 

JozefKozon_1-1736926298164.png

JozefKozon_2-1736926341878.png

I have measured about that voltage on the BUCK1 and BUCK3 with multimeter. 0.91V and 0.81V. 

With Best Regards,

Jozef

 

 

0 件の賞賛
返信

3,669件の閲覧回数
Michaelscott237
Contributor I
Also it seems that nothing that i do changes something in buck3, it always stays 0.89-0.91
0 件の賞賛
返信

3,666件の閲覧回数
Michaelscott237
Contributor I
Correction, the output of buck3 is only rising up
0 件の賞賛
返信

3,646件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hey Michael,

I apologize for a late reply. I have tested my EVB again and from the beginning the voltages were as in my previous answer, but if I left the board running for a while the BUCK3 output voltage raised from 0.81V to above 1V. Another customer placed a very same question. My colleague escalated the PCA9541 single phase configuration question to an application team in our internal community. Let's please wait for an answer from the application team to the other customer's question and I will post it here as soon as they will answer.

Thank you for your patience. 

With Best Regards,

Jozef

0 件の賞賛
返信

3,639件の閲覧回数
Michaelscott237
Contributor I
Thanks for the reply, will wait for an answer
0 件の賞賛
返信

3,630件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Michael,

I have checked the internal community and the application engineer has answered to my colleague. Unfortunately the PCA9451 is indeed not suitable for single phase. I apologize for inconvenience. 

DESCRIPTION

For the PCA9451A device,  user must use dual phase work of BUCK1&3. 

With Best Regards,

Jozef

0 件の賞賛
返信

3,623件の閲覧回数
Michaelscott237
Contributor I
I see, thank you
0 件の賞賛
返信