PF8121 configuration files for the standard types EU/F1/F2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF8121 configuration files for the standard types EU/F1/F2

6,037件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

Customer :  Larslabs  (Germany)

Platform:     i.MX 8M-Mini + PF8121

 

jinyuzhang

 

Hi Jinyu, one of my customers got a few unprogrammed  PF8121 samples (programmed samples were not available) and need to program them now with our FlexGUI utility.

 

Can you please supply me with the config files for the standard configurations?

It would be nice to use them as templates and apply minor changes.

 

Another question arises when looking at the configuration report of the EU device. From the configuration point of view this seems to be the device which is used in the schematic of Boundary Devices for the Nitrogen board.
But in this schematic SW3 and SW4 are connected together for VDD_ARM. The report says that the EU starts up with 0.9V for SW3 and 0.85V for SW4, which doesn't seem to fit.

 

So do you know if one of the configurations EU/F1/F2 fits to the Boundary Devices board?

Regards,

Bernhard.

ラベル(2)
タグ(2)
0 件の賞賛
返信
6 返答(返信)

5,769件の閲覧回数
jinyuzhang
NXP Employee
NXP Employee

Hi 

    I check the website of Boundary, the schematic is updated and may customer should refer to the one below:

    https://boundarydevices.com/product/nitrogen8m-mini/ 

    and it should use the EU standard version.

BRs

jinyu  

PMIC and SBC question
0 件の賞賛
返信

5,765件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

Hi wenhuachen‌, the customer had an older version of the schematic (attached).

In fact there was another question in my initial request:

Can you please supply me with the config files for the standard configurations?

Then the customer can use the config file for the EU and make the required minor modifications and program the A0 samples he has.

Thanks,

Bernhard.

0 件の賞賛
返信

5,765件の閲覧回数
wenhuachen
NXP Employee
NXP Employee

bernhardfink

Please see attached.

0 件の賞賛
返信

5,765件の閲覧回数
wenhuachen
NXP Employee
NXP Employee

bernhardfink

Can you please share schematic of Boundary Devices board you are referring to? BD has many version, EU should match the latest version but I don't know which one BD is published.

0 件の賞賛
返信

5,765件の閲覧回数
jinyuzhang
NXP Employee
NXP Employee

Hi Winni 

   Do you have some comments about this issue?wenhuachen 

BRs

jinyu

PMIC and SBC question
0 件の賞賛
返信

5,765件の閲覧回数
wenhuachen
NXP Employee
NXP Employee

Hi Jinyu,

It should be E8, I will talk with team whether E8 can be set as a standard PN. Thanks.jinyuzhang

0 件の賞賛
返信