PF3000 no need Standby control(with I.MX7)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF3000 no need Standby control(with I.MX7)

Jump to solution
1,707 Views
HOTA
Contributor III

Hi,

I am considering using the combination of PF3000 and I.MX7. For the power specifications, we are considering simple operation with just ON/OFF.

① In this case, I am considering fixing the STANDBY(4PIN) of PF3000 to Low at all times, and controlling PWRON(48PIN) to High/Low to turn the power On/Off. Is this understanding correct?

② Even if I set PWRON(48PIN) to Low (power OFF), is it correct to understand that VSNVS(34pin) will continue to be output?

 

③I am considering using it by supplying 3.0 to 4.0V to VIN without a coin cell. If VIN is 3.0V, should I understand that VSNVS will be about 2.89V from the spec of VSNVSDROP? Unlike other LDOs, there is no graph of Dropout Voltage of VSNVS in the specification, but could you tell me if there is any data depending on temperature or something else?(LICELL(36pin) connected VLDO1_1V8)

Thanks,

Tags (1)
0 Kudos
Reply
1 Solution
1,617 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:

guoweisun_0-1692595232095.png

3: If VIN=3.0V without coincell the default output is 3.0V but should have 110mV drop.

 

 

View solution in original post

0 Kudos
Reply
4 Replies
1,666 Views
guoweisun
NXP TechSupport
NXP TechSupport

① In this case, I am considering fixing the STANDBY(4PIN) of PF3000 to Low at all times, and controlling PWRON(48PIN) to High/Low to turn the power On/Off. Is this understanding correct? [gw]You can configure PMIC on active standby mode by below picture:

② Even if I set PWRON(48PIN) to Low (power OFF), is it correct to understand that VSNVS(34pin) will continue to be output?

[gw]Yes.

③I am considering using it by supplying 3.0 to 4.0V to VIN without a coin cell. If VIN is 3.0V, should I understand that VSNVS will be about 2.89V from the spec of VSNVSDROP? Unlike other LDOs, there is no graph of Dropout Voltage of VSNVS in the specification, but could you tell me if there is any data depending on temperature or something else?(LICELL(36pin) connected VLDO1_1V8)

[gw]When powered by VIN, VSNVS is an LDO capable of supplying 3.0 V.

0 Kudos
Reply
1,630 Views
HOTA
Contributor III

Hi,

Thank you for your response.
① I didn't see a diagram. Could you please provide one?
② I understand. Thank you.
③ So, even if the voltage supplied to VIN is 3.0V, VSENS will output 3.0V without a dropout, is that correct?

Thanks,

HOTA

0 Kudos
Reply
1,618 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:

guoweisun_0-1692595232095.png

3: If VIN=3.0V without coincell the default output is 3.0V but should have 110mV drop.

 

 

0 Kudos
Reply
1,593 Views
HOTA
Contributor III

Hi guoweisun,

Thank you for your response.

 I understand. Thank you.

Thanks,

HOTA

0 Kudos
Reply