PF1550 supplied from an external source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF1550 supplied from an external source

ソリューションへジャンプ
2,022件の閲覧回数
Davide91
Contributor I

Hello,

There is something I cannot understand from PF1550 datasheet: can the PMIC be supplied from an external source, even if the battery is present and being loaded?

How does the VSYS voltage interact with the battery charge? Is it possible to provide VSYS from an external source?

Thanks

Davide

0 件の賞賛
返信
1 解決策
2,012件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Davide,

 

Yes, the PMIC be supplied from an external source, even if the battery is present and being loaded, use external 5.0V from USB on VBUSIN.

 

VSYS voltage interact with the battery charge. VSYSMIN parameter sets the point where the VSYS loop starts taking control and regulates the output. 4.3 V is the recommended setting to ensure that there is enough headroom before reaching UVDET.

Check Figure 17 of the datasheet that shows the charging profile for a better understanding of the relationship between VSYS and the battery charge.

 

Do not connect external source to VSYS.

 

Regards,

Jose

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,013件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Davide,

 

Yes, the PMIC be supplied from an external source, even if the battery is present and being loaded, use external 5.0V from USB on VBUSIN.

 

VSYS voltage interact with the battery charge. VSYSMIN parameter sets the point where the VSYS loop starts taking control and regulates the output. 4.3 V is the recommended setting to ensure that there is enough headroom before reaching UVDET.

Check Figure 17 of the datasheet that shows the charging profile for a better understanding of the relationship between VSYS and the battery charge.

 

Do not connect external source to VSYS.

 

Regards,

Jose

0 件の賞賛
返信