PCA9451A / imx93 battery backup for RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9451A / imx93 battery backup for RTC

2,020件の閲覧回数
arekkaras
Contributor III

Hello,

 

does the PCA9451A support battery backup for NVCC_BBSM_1V8 voltage domain ?

Is there any application note/recommendation how to keep RTC running on iMX93 while there is no external 5V power supply connected to PMIC?

 

Regards
Arkadiusz

0 件の賞賛
返信
3 返答(返信)

1,982件の閲覧回数
arekkaras
Contributor III

Hi Guoweisun,

It was my first idea, but I realised that from this input also other LDO's are powered so it doesn't seem to be best solution.

Additionally, I am using 32kHZ RTC clock from PMIC for iMX93 as well, so in order to get this clock running IMHO whole PMIC needs to be powered ?

 

Regards

Arkadiusz

 

 

0 件の賞賛
返信

1,968件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Yes,correct!

0 件の賞賛
返信

2,000件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

Do you mean that use battery as input of LDO1 to get the backup power?

guoweisun_0-1713249285436.pngguoweisun_0-1713249285436.png

 

0 件の賞賛
返信