PCA9451A / imx93 battery backup for RTC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9451A / imx93 battery backup for RTC

2,080 Views
arekkaras
Contributor III

Hello,

 

does the PCA9451A support battery backup for NVCC_BBSM_1V8 voltage domain ?

Is there any application note/recommendation how to keep RTC running on iMX93 while there is no external 5V power supply connected to PMIC?

 

Regards
Arkadiusz

0 Kudos
Reply
3 Replies

2,042 Views
arekkaras
Contributor III

Hi Guoweisun,

It was my first idea, but I realised that from this input also other LDO's are powered so it doesn't seem to be best solution.

Additionally, I am using 32kHZ RTC clock from PMIC for iMX93 as well, so in order to get this clock running IMHO whole PMIC needs to be powered ?

 

Regards

Arkadiusz

 

 

0 Kudos
Reply

2,028 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Yes,correct!

0 Kudos
Reply

2,060 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

Do you mean that use battery as input of LDO1 to get the backup power?

guoweisun_0-1713249285436.png

 

0 Kudos
Reply