PCA9450CHNY LOADSW_CTRL Register

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCA9450CHNY LOADSW_CTRL Register

跳至解决方案
3,156 次查看
omar_wolfe-huss
Contributor III

I am seeing behaviour on the LOADSW_CTRL register (0x2A) of PCA9450CHNY that doesn't match the documentation. In table 64 of the datasheet is shows the reset state of the register is 0x85, which allows SW_EN to control the state of the load switch. We are seeing that devices actually power up with a default state of 0x84, which sets the load switch to "Always off". Is this expected?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,145 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Omar,

Indeed, the default value of the LOADSW_CTRL register should be 0x85.

In this case, I assume the device is detecting a short circuit current based on the SW_SC bit as follow:

diazmarin09_0-1644372299740.png

 

As a test, could you please set this bit (SW_SC) to 1? If the device restarts in 100ms, indeed, the switch is detecting a short circuit.

Please let me know the results.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,122 次查看
omar_wolfe-huss
Contributor III

Hi David,

 

Many thanks for your suggestion. When I change SW_SC to 1 I can see that the power is up after 100ms, confirming that a short circuit is being detected. This appears to be in-rush and so we will amend the design to prevent this from happening.

0 项奖励
回复
3,146 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Omar,

Indeed, the default value of the LOADSW_CTRL register should be 0x85.

In this case, I assume the device is detecting a short circuit current based on the SW_SC bit as follow:

diazmarin09_0-1644372299740.png

 

As a test, could you please set this bit (SW_SC) to 1? If the device restarts in 100ms, indeed, the switch is detecting a short circuit.

Please let me know the results.

Regards,

David

0 项奖励
回复