PCA9450AA Production Status?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9450AA Production Status?

Jump to solution
3,745 Views
adevries
Contributor V

Hello,

Can anyone from NXP tell me what the production status of PCA9450AA is? I am developing a product that uses the 8M Mini application processor, and I was interested in using PCA9450AA as a PMIC for it. However, it doesn't look like this part is in stock at any distributors, so to buy any you need to order a whole reel with a lead time of 52 weeks. However, the other variants of PCA9450, PCA9450B and PCA9450C, are both stocked at digikey. Is there any plan to make the PCA9450AA available at lower minimum quantities?

 

Also, it looks like PCA9450A might also work as a PMIC for the 8M Mini. Does anyone know what the difference is between the PCA9450A and PCA9450AA?

 

Thanks

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,734 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

PCA9450AA can fully replace with PCA9450A.

For PCA9450AA supply channel/lead time ,please contact with local NXP distributors.

 

View solution in original post

0 Kudos
Reply
4 Replies
3,629 Views
lumen
Contributor III

Hi,

I see the lead time of the PCA9450B is similar to the PCA9450A/PCA9450AA. From the technical point of view, what is needed that the i.MX8M Mini is working with the PCA9450B?

Best Regards,

Patrick

0 Kudos
Reply
3,735 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

PCA9450AA can fully replace with PCA9450A.

For PCA9450AA supply channel/lead time ,please contact with local NXP distributors.

 

0 Kudos
Reply
3,647 Views
lumen
Contributor III

Hi guoweisun,

The lead time of the PCA9450A seems the be also around 52 weeks.

We are using the i.MX8M Mini without the GPU similar to the i.MX8M Nano. Is it possible to somehow use the PCA9450B instead of the PCA9450AA? What changes must be done on BSP side to configure the PCA9450B correctly for the i.MX8M Mini.

Best Regards,

Patrick

0 Kudos
Reply
3,641 Views
guoweisun
NXP TechSupport
NXP TechSupport
HI PCA9450B is also have a Lead Time: 52.
0 Kudos
Reply