PCA9420 Battery detection in-progress ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9420 Battery detection in-progress ?

12,007件の閲覧回数
akckwang
Contributor I

Hi,

Our device adopts PCA9420UKZ to be pmic,
and charging source is Qi wireless charging,

When we charging battery by Qi wlc charger,
if antennas aren't aligned very accurately,
even charger feels everhthing is right and keep power output,

the pca9420 would stop charging because it falled into a state "Battery detection in-progress",
(CHG_STATUS_2(1Ah) = 0x10, "Battery detection in-progress", "Charger in Idle State")

but at the sametime, register reveals pca9420 has detected battery,
(CHG_STATUS_0(18h) = 0xf0, "VBAT_DET_OK = 1", "VBAT_OK = 1")

Detailed register values:

0x01=0x00, 0x02=0x00, 0x03=0x3f, 0x04=0x00,
0x05=0x7f, 0x06=0x00, 0x07=0xff, 0x08=0xff,
0x09=0x41, 0x0a=0x81, 0x0b=0xce, 0x0c=0x01,
0x0d=0x00, 0x10=0xaf, 0x11=0x14, 0x12=0x02,
0x13=0x13, 0x14=0x0a, 0x15=0x25, 0x16=0x95,
0x17=0x24, 0x18=0xf0, 0x19=0xc0, 0x1a=0x10,
0x1b=0x00, 0x20=0x10, 0x21=0x00, 0x22=0x14,
0x23=0x2c, 0x24=0x41, 0x25=0x2c, 0x26=0x1c,
0x27=0x4c, 0x28=0x4f, 0x29=0x0c, 0x2a=0x1c,
0x2b=0x4c, 0x2c=0x4f, 0x2d=0x0c, 0x2e=0x1c,
0x2f=0x4c, 0x30=0x4f, 0x31=0x0c

datasheet of pca9420 mentioned the battery detection sqquence at "Figure 10. Charger state diagram", 
but we still have no idea how pca9420 to have suceh state,
because seems the voltage we measured doesn't match the conditions of document description,

So we do like to consult more detailed of the "Battery detection in-progress",
How it happened?
Do we have way to know the truly VBAT voltage what pca9420 detected?
Any suggestion to investigate more forward?

2022-09-30:
Try to measure VBAT voltage by oscilloscope,
the voltage has ~0.1V gap between 2 case,
but when wlc charger isn't aligned perfectly, the frquency is ~37Hz only,
compare to aligned perfectly case, the frequency is very low,
is't caused pca9420 can't detect battery?

Thanks~

タグ(1)
0 件の賞賛
返信
5 返答(返信)

11,984件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

The device has a unique battery detection scheme with two comparators, 1.9V and 3.4V.
when the detection scheme is executed, a 5mA current sink is activated to determine
battery presence by detection the fall threshold, VBAT_DET_LOW, 1.9V typ. In addition,
a 5mA current source is used to detect battery voltage whether it stays above the
threshold, VBAT_DET_UP, 3.4V. if both conditions are met, absence of battery is declared.

0 件の賞賛
返信

11,941件の閲覧回数
akckwang
Contributor I

Hi @guoweisun,

If VBAT freuency drop to ~37Hz, can pca9420 still detect battery normally?

We measured VBAT by oscilloscope,
and noticed that when wlc charger isn't aligned perfectly,
the VBAT voltage has ~0.1V drop compare to normal case,
but frequency is droped to ~37Hz.

Thanks~

0 件の賞賛
返信

11,913件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Vbat should be clear DC voltage, don't understand why it has the frequency in your side.

 

0 件の賞賛
返信

11,907件の閲覧回数
akckwang
Contributor I

Hi @guoweisun,

Can pca9420 battery detection work with the "strange frequency" dc voltage?

Thanks~

0 件の賞賛
返信

11,974件の閲覧回数
akckwang
Contributor I

Hi Guoweisun,
Your reply is exactly what pca9420 document Figured 10 mentioned,
and that can't explain why our pca9420 can't detect battery event VBAT is stable ~3.9V...

0 件の賞賛
返信