Output Ripple VR5100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,421件の閲覧回数
joe1652
Contributor IV

Hello, for the VR5100 the datasheet on page 12 shows an output ripple of 5mV, is that peak to peak?

Thanks,

Joe

0 件の賞賛
返信
1 解決策
2,360件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Joe,

You are correct, the 5mV of the output ripple of the Buck registers should be marked as peak-to-peak voltage (5mVp-p).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,361件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Joe,

You are correct, the 5mV of the output ripple of the Buck registers should be marked as peak-to-peak voltage (5mVp-p).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------