Output Ripple VR5100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output Ripple VR5100

Jump to solution
2,419 Views
joe1652
Contributor IV

Hello, for the VR5100 the datasheet on page 12 shows an output ripple of 5mV, is that peak to peak?

Thanks,

Joe

0 Kudos
Reply
1 Solution
2,358 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Joe,

You are correct, the 5mV of the output ripple of the Buck registers should be marked as peak-to-peak voltage (5mVp-p).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
2,359 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Joe,

You are correct, the 5mV of the output ripple of the Buck registers should be marked as peak-to-peak voltage (5mVp-p).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------