Output Ripple VR5100

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Output Ripple VR5100

跳至解决方案
2,431 次查看
joe1652
Contributor IV

Hello, for the VR5100 the datasheet on page 12 shows an output ripple of 5mV, is that peak to peak?

Thanks,

Joe

0 项奖励
回复
1 解答
2,370 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Joe,

You are correct, the 5mV of the output ripple of the Buck registers should be marked as peak-to-peak voltage (5mVp-p).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,371 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Joe,

You are correct, the 5mV of the output ripple of the Buck registers should be marked as peak-to-peak voltage (5mVp-p).


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------