MMPF0100AEP Power On Procedure/Solution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100AEP Power On Procedure/Solution

2,066件の閲覧回数
azhagiri_sadago
Contributor I

Hello,

I am using MMPF0100AEP PMIC for i.MX6 Quad Processor based board.

I have referred the Power section from SABRE design files,

I am unable to get the PMIC outputs

Kindly suggest the detailed power on procedure of PMIC.

And also please share the detailed information about OTP configuration, please let me know about powering on the PMIC using Hardcode.

Thank You

Regards,

Azhagiri

ラベル(3)
0 件の賞賛
返信
1 返信

1,948件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Azhagiri,

I believe that the part number that you are referring to is the MMPF0100F0AEP. In the datasheet and the application note AN4536, you will find start-up with hard-coded configuration as well as OTP programming instructions.

I hope this information can be helpful. Please let me know if you have further questions.

Have a great day,

Paulina

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信