MC56F8345VFGE date code marking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8345VFGE date code marking

3,738件の閲覧回数
melmoss
Contributor I

 

I am looking for an explanation between the differences of the date code markings on these 2 parts. I think the Reference datecode XAC1742D was made in 2017, week 42 and the TTE08 XAA2245C was made in 2022, week 45. The 3rd character and the last character are different on each device and I cannot easily find an explanation as to what these characters mean? Is there a document that explains date code markings on these parts? The part labelled TTE08 has been returned from the field this year

 

melmoss_0-1689059581502.png

 

0 件の賞賛
返信
3 返答(返信)

3,726件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You are right, for the "XAC1742D", it was manufactured at 2017 year week 42. For the "XAA2245C", it was manufactured at 2022 year week 45.  For the "XAC", "XAA", they are internal code.

Hope it is helpful

BR

XiangJun Rong

0 件の賞賛
返信

3,712件の閲覧回数
melmoss
Contributor I

Thank you for the feedback. Much appreciated. To complete my query are the last characters D and C on the data codes for internal use only as well?

0 件の賞賛
返信

3,699件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Yes, the last character "C" and "D"  are also internal code, the Chip Revision is only represented by the date code.

BR

XiangJun Rong

0 件の賞賛
返信