MC34VR500V8ES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC34VR500V8ES

3,040件の閲覧回数
Urmila_123
Contributor II

Hello Everyone,

This PMIC device MC34VR500V8ES is used in LS1046ARDB. is that used as per default settings or programmed using I2C. Please Reply.

Thanks & Regards

Urmila.

0 件の賞賛
返信
5 返答(返信)

3,034件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Urmila,

please refer to the Table 1. in the MC34VR500 datasheet. The MC34VR500V8ES version is preprogrammed to be used with the LS1046A Processor. If you buy the MC34VR500V8ES version, the regulators (Buck regulators, LDOs) are set to fit the LS1046A Processor requirements.

With Best Regards,

Jozef

3,022件の閲覧回数
Urmila_123
Contributor II

Thank you Jozef.

I have one more query. Hope you clarify.

In fig 5 : Starting sequence of MC34VR500 data sheet, it was shown that SW3 and SW4  regulators output the voltages 1.8V and 1V (default values respectively) at the same time. is this applicable to MC34VR500V8ES also? Please confirm.

With Best Regards

Urmila P.

0 件の賞賛
返信

3,010件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Urmila,

yes, that is correct. The SW3 and SW4 voltage levels for the MC34VR500V8ES version are 1.8V and 1.0V respectively. 

JozefKozon_0-1633524272122.png

 

With Best Regards,

Jozef

3,003件の閲覧回数
Urmila_123
Contributor II

Yeah Jozef. will there be any delay between SW3 and Sw4 outputs? I am talking sequencing.

Regards

Urmila P.

 

0 件の賞賛
返信

2,997件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Urmila,

please refer to the Figure 5. in the datasheet. The SW3 and SW4 will be turned on at the same time.

JozefKozon_0-1633585272049.png

With Best Regards,

Jozef

0 件の賞賛
返信