MC33PF8200A0ES usage for LS1043A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33PF8200A0ES usage for LS1043A

1,560 Views
arif_kanganolli
Contributor I

Hello Team,

I need a input for using PMIC-MC33PF8200A0ES with LS1043A processor, I need a PMIC which has programmed and can be used directly with my LS1043A processor.

Another option if I need to program what tools I require and what is the HW configuration should be followed.

Provide me confirmation for the same

Thanks & Regards,

Arif

Labels (1)
0 Kudos
Reply
1 Reply

1,443 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Arif:

The NXP PMIC part number MC33PF8200CXES is preprogrammed to be used directly with the LS1043A without the need of any extra programming on the PMIC.

You can find all the OTP configuration (sequence, voltage rails, etc.) for this part number in the following link: https://www.nxp.com/docs/en/supporting-information/R_PF8200CX.PDF?tid=MC33PF8200CXES-OTP-Report


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply