MC33774ASP1AE Cell Balancing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33774ASP1AE Cell Balancing

3,103件の閲覧回数
mohanagv
Contributor II

As per the NDA MC33774AESP1AE datasheet

mohanagv_0-1724830294732.png

1.Is it possible to combine constant current mode with other balancing modes? If yes, does BAL_STAT0.CHx (the bit reflecting that the channel is under balancing mode) affect constant current balancing? If no, what is the stop condition for constant current balancing?
2. What is the value of VCellmin, VCell in PWMDUTYCYCLE=VCellmin/ VCell.? 
MC33774  

タグ(1)
3 返答(返信)

3,074件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Mohana,

1.Is it possible to combine constant current mode with other balancing modes? If yes, does BAL_STAT0.CHx (the bit reflecting that the channel is under balancing mode) affect constant current balancing? If no, what is the stop condition for constant current balancing?

[A] Please refer to the AN14084. The balancing modes are very well described there. The balancing modes can be combined. E.g. the Voltage-controlled balancing and Temperature-controlled balancing. Please download the AN14084 from the MC33774A product page, under the secure files.

JozefKozon_0-1724842065760.png

2. What is the value of VCellmin, VCell in PWMDUTYCYCLE=VCellmin/ VCell.? 

Could you please direct me to the formula you are referring to? So far I couldn't find it in available documents.

 

With Best Regards,

Jozef

3,066件の閲覧回数
mohanagv
Contributor II

1.In the product path below, I am able to find only 5 secure files, and the AN14084 document is not there.
https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/18-channel... 

mohanagv_0-1724845017758.png

 

2.Regarding the formula, it is in the constant current balancing section of the MC33774A datasheet.
constant current balancing.png

Regards

Mohana G V

0 件の賞賛
返信

3,050件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Mohana,

you need to ask for a higher access. My colleague supported your colleague via chat.

The minimum Cell voltage for the MC33774A is 2.0V. Below this, the UV is triggered.

JozefKozon_0-1724915466023.png

With Best Regards,

Jozef

 

タグ(1)