MC33664 TPL data bits 0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC33664 TPL data bits 0

跳至解决方案
797 次查看
divyam
Contributor II

Hi,

I'm trying to communicate to MC33771 AFE and while debugging i noticed that whatever I send on MOSI_TX, the TPL waveform bits are logic 0 only (attached waveform)


tpl_0_data.png

image.png

Also: -

1. Wakeup function is working properly. When TPL wakeup command is sent, VCOM changes from 0V to 5V 
2. Waiting for 5msec after sending the wakeup command, before sending any command on SPI_TX 
3. Trying to debug BCC_AssignCid(), whatever data is being sent on SPI_MOSI_TX, TPL shows 0 logic pulses only (corresponding to SPI RX waveform)

Right now i want to focus on the MC33664 transceiver only.
The transceiver should transmit the corresponding data on the bus, in both the cases (AFE present, AFE absent) ?

MC33664

0 项奖励
回复
1 解答
743 次查看
divyam
Contributor II

Hi Jozef,

We tested the same on another hardware.
(Vio = 3.29V, VCC5 = 5.01V)

The data bit stream is OK in that.

This thread can be closed.


在原帖中查看解决方案

0 项奖励
回复
3 回复数
783 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Divyam,

please share your schematic with voltage levels and part values.

With Best Regards,

Jozef

0 项奖励
回复
744 次查看
divyam
Contributor II

Hi Jozef,

We tested the same on another hardware.
(Vio = 3.29V, VCC5 = 5.01V)

The data bit stream is OK in that.

This thread can be closed.


0 项奖励
回复
777 次查看
divyam
Contributor II

Hi Jozef,

Please find the info below:

tpl_sch.png

VCC5     = 4.88V
VIO        = 3.25V
RDTX+  = 2.51V (idle)
RDTX-   = 2.49V (idle)

The waveform shown previously is b/w (RDTX+ and RDTX- after the signal transformer, on the AFE side)

MPN = MC33664ATL1EG

标记 (1)
0 项奖励
回复