MC33664 TPL data bits 0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33664 TPL data bits 0

ソリューションへジャンプ
1,774件の閲覧回数
divyam
Contributor II

Hi,

I'm trying to communicate to MC33771 AFE and while debugging i noticed that whatever I send on MOSI_TX, the TPL waveform bits are logic 0 only (attached waveform)


tpl_0_data.png

image.png

Also: -

1. Wakeup function is working properly. When TPL wakeup command is sent, VCOM changes from 0V to 5V 
2. Waiting for 5msec after sending the wakeup command, before sending any command on SPI_TX 
3. Trying to debug BCC_AssignCid(), whatever data is being sent on SPI_MOSI_TX, TPL shows 0 logic pulses only (corresponding to SPI RX waveform)

Right now i want to focus on the MC33664 transceiver only.
The transceiver should transmit the corresponding data on the bus, in both the cases (AFE present, AFE absent) ?

MC33664

0 件の賞賛
返信
1 解決策
1,720件の閲覧回数
divyam
Contributor II

Hi Jozef,

We tested the same on another hardware.
(Vio = 3.29V, VCC5 = 5.01V)

The data bit stream is OK in that.

This thread can be closed.


元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,760件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Divyam,

please share your schematic with voltage levels and part values.

With Best Regards,

Jozef

0 件の賞賛
返信
1,721件の閲覧回数
divyam
Contributor II

Hi Jozef,

We tested the same on another hardware.
(Vio = 3.29V, VCC5 = 5.01V)

The data bit stream is OK in that.

This thread can be closed.


0 件の賞賛
返信
1,754件の閲覧回数
divyam
Contributor II

Hi Jozef,

Please find the info below:

tpl_sch.png

VCC5     = 4.88V
VIO        = 3.25V
RDTX+  = 2.51V (idle)
RDTX-   = 2.49V (idle)

The waveform shown previously is b/w (RDTX+ and RDTX- after the signal transformer, on the AFE side)

MPN = MC33664ATL1EG

タグ(1)
0 件の賞賛
返信