Is VREFDDR disabled by default?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is VREFDDR disabled by default?

1,218 Views
ghazanhaider
Contributor I

I plan to use MMPF0100 F0 mode. (Part MMPF0100F0ANES)

I plan to use the VREFDDR voltage follower feature for DDR3(L) instead of using resistors as a voltage divider for DDR_VREF

 

The datasheet for PF0100's VREFDDCRTL register on page 26, it says:

"Enable or disables VREFDDR output voltage • 0 = VREFDDR Disabled • 1 = VREFDDR Enabled "

And under the "Default" column the setting is 0x0

 

However the Device Start-up Configuration page (18) shows both the 'Default configuration' and 'F0' modes having the VREFDDR_SEQ set to '3' with no mention of it being enabled or disabled.

 

Q1: Is the VREFDDR output disabled for modes 'default' and 'F0' or will it come up at sequence 3?

Q2: If it is disabled, is the intention for the controlling device (U-Boot) to start up using sram alone, contain PFUZE100 drivers and devicetree and enable VREFDDR?

Q3: If it is disabled, which other part number of PF0100 has it enabled by default?

Labels (2)
0 Kudos
Reply
2 Replies

1,213 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI 

Q1: Is the VREFDDR output disabled for modes 'default' and 'F0' or will it come up at sequence 3?

--Following F0

Q2: If it is disabled, is the intention for the controlling device (U-Boot) to start up using sram alone, contain PFUZE100 drivers and devicetree and enable VREFDDR?

--xxx

Q3: If it is disabled, which other part number of PF0100 has it enabled by default?

--xxx

0 Kudos
Reply

1,203 Views
ghazanhaider
Contributor I
Please clarify:
"Following F0"
Does this mean VREFDDR is enabled in F0 parts?
0 Kudos
Reply