Hi @guoweisun ,
We are currently encountering a severe issue where the balancing IC is getting damaged during the sequential connection of multiple battery cell groups.
Following the local NXP technical advice regarding the unused channels on our Group 1 section (which monitors 14 cells), we have terminated the unused pins as follows directly at the balancing IC input:
- Connected CB15-18 shorted to CB14
- Connected CT15-18 shorted to CT14
Here are the details of our test procedures and the corresponding outcomes:
Test 1: Single Group Connection (Group 1 Only)
Procedure: We connected only Group 1, which corresponds to the highest potential segment: Cell 37 to Cell 50 (Total of 14 cells, total voltage approx. 50V).
Result: The board functioned normally. We were able to accurately read the voltages of all cells. The measured voltage of VBAT_1 relative to GND_1 was stable at approximately 50V. No anomalies were observed.
Test 2: Full 3-Group Connection (Sequential Power-Up)
Procedure: We connected all 3 cell groups simultaneously but followed a strict bottom-to-top insertion sequence, starting from Group 3 (bottom cells) up to Group 1 (top cells).
Result: Upon completion of the connection, smoke and a visible burn occurred near resistor R1_1 (10 ohm). We immediately cut off the power supply to prevent further damage and inspected the board.
Post-Mortem & Damage Analysis:
- VBAT_1 to GND_1 Short Circuit: Electrical testing revealed a dead short between VBAT_1 and GND_1. Since this power line feeds directly into the balancing IC, we suspected internal silicon failure.
- Resistor R1_1: The 10 ohm resistor was found to be blown open (open-circuit).
- CT & CB Pins: Inspected both CT and CB pins; there was no physical or electrical damage detected on these pins.
- Balancing Resistors: Inspected all external cell-balancing resistors; all remain intact and undamaged.
- IC Root Cause Verification: We desoldered the balancing IC from the PCB to isolate the issue. Testing the unmounted IC confirmed a permanent internal short circuit between the VBAT and GND pins.
Questions for NXP Support:
- Given that the configuration works flawlessly when Group 1 is powered up individually, what could trigger an internal VBAT-to-GND breakdown inside the balancing IC when all three groups are plugged in sequentially (from bottom to top)?
- Could the termination method of shorting the unused pins (CB15-18 to CB14, and CT15-18 to CT14) induce unexpected transient states or latch-up conditions during multi-chip daisy-chain hot-plugging?
- What specific hot-plug protection, TVS adjustments, or power-up sequencing constraints do we need to implement to mitigate this failure mode?
Please help us analyze and recommend ways to resolve this issue
CMU_1st_group_damage.jpg