Info related to usage of PMIC(VR5510) for S32K148 Eval Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Info related to usage of PMIC(VR5510) for S32K148 Eval Board

2,379 Views
satish_k_singh
Contributor III

Hello ,

Currently i am planning to use the PMIC (VR5510) to connect to S32K148.. by using the I2C.

So could you please let know where can I find the information related to the same.

from the info i have got ,

I have the below queries : 

1. I understand that the I2C driver is implemented as Complex device driver and not following the complete Stack layer in the AUTOSAR MCAL (S32K14X_MCAL_4.2_RTM_P4_1.0.1) which is currently available. Kindly let know if my understanding is right or do we already have the I2C driver which is available following the AUTOSAR 4.2.

2.Could you please let know if we already have some sample program which can be used as reference to interface the PMIC to the S32K148 Eval Board.

 

thanks and best regards!!!

0 Kudos
Reply
1 Reply

1,848 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

in case of Autosar/MCAL question, it's better to create a ticket for our SW team:

http://nxpcommunity.force.com/community/CommunityContextPage 

I got information that there are no drivers or code example yet.

Regards,

Lukas

0 Kudos
Reply