How to program FS26 with KITFS26SKTEVM evaluation board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to program FS26 with KITFS26SKTEVM evaluation board

Jump to solution
598 Views
simon98
Contributor III

Hi NXP Team,

I was trying to program a MFS2630AMDA0AD using the KITFS26SKTEVM evaluation board.

I've followed all the steps of the NXP GUI for FS26 Automotive PMIC Family user manual at chapter 7.4 "Device programming" and chapter 8.5" Programming the device with an OTP configuration"...

When i click program the GUI pops me up this message:

 

program_otp_fs26_problem.png

I've noticed that the user manual in chaper 7.4 mentions the Jumper J13 that is not present on my evaluation board.

Where do i have to focus on in order being able to program my device?

 

Thanks a lot,

Simon

Tags (1)
0 Kudos
Reply
1 Solution
581 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello

Please see following steps:

It is recommended to set your power supply to an initial value of 12V and current limited to 0.5A.

  1. Make sure SW1 is OFF (middle position)
  2. Plug the USB cable into the “USB KL25Z” port
  3. Switch SW7 ON (DBG = 8V)
  4. Plug the power supply on J21 and switch SW1 on the left side
  5. You’re now in OTP Mode. LEDs status should be the same than the picture
  6. Open the graphic user interface
  7. Click on FS26-C0 and “OK” button
  8. Click on “Start” button to start the communication
  9. Verify FS_STATES is “4-Debug entry”
  10. Click on PROG tab on the left panel
  11. Click on « Apply test mode» button.
  12. Click on « Read » button to know the fuse box status
  13. Click on « Browse » button and the select the OTP script

At this step, the product is ready to be programmed

FS26OTP.jpg

Hope this helps.

View solution in original post

0 Kudos
Reply
1 Reply
582 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello

Please see following steps:

It is recommended to set your power supply to an initial value of 12V and current limited to 0.5A.

  1. Make sure SW1 is OFF (middle position)
  2. Plug the USB cable into the “USB KL25Z” port
  3. Switch SW7 ON (DBG = 8V)
  4. Plug the power supply on J21 and switch SW1 on the left side
  5. You’re now in OTP Mode. LEDs status should be the same than the picture
  6. Open the graphic user interface
  7. Click on FS26-C0 and “OK” button
  8. Click on “Start” button to start the communication
  9. Verify FS_STATES is “4-Debug entry”
  10. Click on PROG tab on the left panel
  11. Click on « Apply test mode» button.
  12. Click on « Read » button to know the fuse box status
  13. Click on « Browse » button and the select the OTP script

At this step, the product is ready to be programmed

FS26OTP.jpg

Hope this helps.

0 Kudos
Reply