How to drive FS26 via LPSPI3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to drive FS26 via LPSPI3?

Jump to solution
3,266 Views
Allen_863
Contributor III

I am using the S32K3X4EVB-T172 for development.

I discovered that I couldn't communicate with the FS26 using LPSPI3, and then I replicated this situation in the example code.

I want to replace

LPSPI3_PCS0 = 110 = PTB17 <> LPSPI0_PCS0 = 95 = PTB0
LPSPI3_SCK = 7 = PTD1 <> LPSPI3_SCK = 7 = PTD1
LPSPI3_SIN = 111 = PTD20 <> LPSPI0_SIN = 97 = PTC9
LPSPI3_SOUT = 8 = PTD0 <> LPSPI0_SOUT = 94 = PTB1

The wiring method is as follows:

LPSPI3_SCK = J37, number 1, connects to LPSPI0_SCK = J2, number 21
LPSPI3_SIN = J39, number 14, connects to LPSPI0_SIN = J2, number 15
LPSPI3_SOUT = J37, number 3, connects to LPSPI0_SOUT = J2, number 18
LPSPI3_PCS0 = J4, number 5, connects to LPSPI0_PCS0 = J2, number 24

20251219_140651.jpg

The known failure point is that Sbc_fs26_GetDeviceState within Sbc_fs26_InitDevice returns FS_STATES_INVALID.

5.png

However, if I use Spi_SyncTransmit, I find that CSB is pulled low, which seems to be correct.

CSB

CSB.jpg

MOSI

MOSI.jpg

I've checked the configuration, and I can't see where the problem is. The attached file is almost identical to the example code, except that LPSPI0 has been changed to LPSPI3.

1.png2.png3.png

Tags (2)
0 Kudos
Reply
1 Solution
3,072 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please note that during the Christmas holiday period, our support response times may be longer than usual. Thank you for your understanding.

我看了您的描述是在做一个SPI 通信移植在我们的RTD上,确实有点超出support的范围了

View solution in original post

0 Kudos
Reply
6 Replies
3,158 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI Allen

您这个属于code移植吗?

0 Kudos
Reply
3,154 Views
Allen_863
Contributor III

不是 CODE 移植,是我有一包 CODE 很大包,我在上面遇到了 LPSPI3 无法与 FS26 沟通的问题,为了方便提问,我用 FS26 的范例代码,把它从 LPSPI0 改成 LPSPI3 和 FS26 沟通,但是也遇到无法用 LPSPI3 与 FS26 沟通的状况,但是呼叫 Spi_SyncTransmit 又可以看到 CSB 与 MOSI 有相对应的反应,所以不知道原因是什麽 ?

Tags (3)
0 Kudos
Reply
3,151 Views
guoweisun
NXP TechSupport
NXP TechSupport

那我们的官方example是用的哪个SPI 跟FS26通信的?

0 Kudos
Reply
3,136 Views
Allen_863
Contributor III

使用 LPSPI0
我有把 LPSPI0 删除,然后进行以下的对接
LPSPI0_PCS0 = 95 = PTB0 = J2 上 24 对接 LPSPI3_PCS0 = 110 = PTB17 = J4 下 5
LPSPI0_SCK = 98 = PTC8 = J2 上 21 对接 LPSPI3_SCK = 7 = PTD1 = J37 上 1
LPSPI0_SIN = 97 = PTC9 = J2 上 15 对接 LPSPI3_SIN = 111 = PTD20 = J39 中 14
LPSPI0_SOUT = 94 = PTB1 = J2 上 18 对接 LPSPI3_SOUT = 8 = PTD0 = J37 上 3
但是 FS26 会无法沟通

Tags (2)
0 Kudos
Reply
3,073 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please note that during the Christmas holiday period, our support response times may be longer than usual. Thank you for your understanding.

我看了您的描述是在做一个SPI 通信移植在我们的RTD上,确实有点超出support的范围了

0 Kudos
Reply
3,075 Views
Allen_863
Contributor III

使用 LPSPI0
LPSPI0_PCS0 = 95 = PTB0
LPSPI0_SCK = 98 = PTC8
LPSPI0_SIN = 97 = PTC9
LPSPI0_SOUT = 94 = PTB1

Tags (2)
0 Kudos
Reply