How To Apply UJA1075ATW Watchdog?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How To Apply UJA1075ATW Watchdog?

3,285件の閲覧回数
alighieri
Contributor III

HELLO

According To Datasheet And Following Diagram Of UJA1075ATW Here Is Not WDI (Watchdog Input) To Be Periodically Kicked. So We're Confused About The Mechanism Of Watchdog Timer. In Our Case We Want To Apply Watchdog For A System Supervisor To Monitor MCU's Status. IF MCU Behave Abnormal Then Reset MCU For 3 Times. After 3-Times Reset Pull EN Pin As High To Turn Off External Gate / Switch For A Prevention That A Power Source Cause Malfunction To Relay / Motors Upon Seat / Sunroof / Mirror.

pastedImage_1.png

Here Are The Questions:

1. What Different From 

UJA1075ATW/5V0/WDJ / UJA1075ATW/5V0WD,1

2. In Datasheet We Don't See Much About Watchdog Timer'ss Mechanism.

We Want To Make Sure Does The Watchdog Support

2-1 Kicking Dog Method - We Designed Our First Engineering Board With Maxim MAX16998AAUA/V+ And Due To Cost Issue We Find NXP SBC Will Be Great Choice In Replacement Of Old Design With 1 LDO / 1 CAN / 1 LIN / 1 Watchdog. Original Design:

MCU Periodically Kick Dog To Prevent Bite-On

Once Timeout The Mentioned Watchdog Will Reset MCU For 3 Times

If MCU Stay In Malfunction Without Kicking Dog Then Set SBC Enable Pin Active High To Turn Off System Power Source For Relay To Motor.

2-1-1. Can We Depend SPI Clock To Judge External MCU's Status Then Decide Timing To Reset The External MCU?

2-1-2. Can We Reset The External MCU When The MCU Is Broken? By RSTN Level?

2-1-3. What If A Situation Like MCU Is Broken And Drop-Down The Level Of WDOFF Will Be?

2-2 We Don't See Any Details About The Built-in Watchdog. First General Watchdog Required To Be Kick But The UJA1075 Seems No WDI (Input Pin). Our Problem Is The Watchdog Can Be Configured By SPI To Register For 3-Time Reset Mechanism? (Enable RSTN Pin To Reset External MCU For 3 Times)

2-3 pastedImage_1.png

Looks Like Dog Kicks Are By SPI TO NWP. Problem Is Here Is Not Register Address Definitions In Datasheet.

3. Any Application Note Has Enough Information For Such A SBC Like UJA1075ATW?

4. Here Is 2 Sets Of Wakeup Pins. What Do Them Purpose On? Any Differences?

5. What Is The LIMP Pin For? I See A Description In Datasheet Tells LIMP Is For Overtemp Protection Use? 

6. Here Is 2 Wakeup Pins Input To SBC. I Wonder What Situation Will Apply 2 Wakeup Pins?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,039件の閲覧回数
alighieri
Contributor III

I've Post My Problem For Time But The Post Still Waiting For Host To Authorize.

Please IT IS Emergent Problem Due To Mass Production Date.

0 件の賞賛
返信

3,039件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Bright,

The only difference between the UJA1075ATW/5V0/WDJ and UJA1075ATW/5V0/WD,1 is manufacturing site. From the application point of view there is no difference.

 

As for the watchdog configuration and behavior, please refer to the UJA1075A datasheet (Chapter 6.4) and AH1002 (Chapter 3.1.2) that was sent to you internally (Case #00184627) yesterday.

 

I strongly recommend to take a closer look at the AH1002 where you should find answers also to your remaining questions. If not, please update the Case #00184627 or this thread.

Best regards,

Tomas

0 件の賞賛
返信

3,039件の閲覧回数
alighieri
Contributor III

Tomas

Is Is A Vital Error To The UJA1075ATW. According To Application Hint When We Tried To Read Device ID We Read Wrong ID Which Is Not Listed In Application Hint. 

We Currently Have 2 Board Designed With Different M0 MCU:

Kinetis EA

S32K116

And Same SBC UJA1075ATW

But In

Kinetis EA Case We Read 0x5002

S32K116 Case We Read 0x5004

We Tried Every Boards By Hand But Always Read The Same Device ID.

IT STRANGE IF THE DEVICE BOUGHT IS WRONG WHY ARE THEM SO REGULAR FOR THE WRONG DEVICE IDS?

0 件の賞賛
返信