Fs26 - ESD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,967件の閲覧回数
harish_crowdnidhi
Contributor III

Dear All,

Can someone share the FS26 internal ESD protection structure?

We are using the device. We would like to be absolutely sure of which pins we need to protect.

Your quick feedback would be much appreciated.

0 件の賞賛
返信
1 解決策
2,933件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

There is more detail ESD protection level introduce in the datasheet, you can refer to this and decide whether need add ESD protection external.

 

guoweisun_0-1693471341721.pngguoweisun_0-1693471341721.png

 

元の投稿で解決策を見る

4 返答(返信)
1,879件の閲覧回数
luzinsk2
Contributor I

What is the recommended esd protection for the ctn730. What about protecting certain pins such as TVDD (Tied to Vuptx).  

 

Any insight to if TVDD, CTX_P are vulnerabe to esd? 

0 件の賞賛
返信
2,960件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Unfortunately we can't share this internal ESD structure to customers, if you have any detail ESD questions you can list here.

 

0 件の賞賛
返信
2,960件の閲覧回数
harish_crowdnidhi
Contributor III

We need it to understand if we have to provide protection to pins from outside or NXP guys have already taken care of it pls.

I hope you are understanding our situation ?.

0 件の賞賛
返信
2,934件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

There is more detail ESD protection level introduce in the datasheet, you can refer to this and decide whether need add ESD protection external.

 

guoweisun_0-1693471341721.pngguoweisun_0-1693471341721.png