FS86 Debug mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS86 Debug mode

2,817 Views
libra_z
Contributor I

hi,

When the FS86 enters DEBUG mode through the DBG pin, can it skip the FS_INIT state without refreshing the watchdog?
At this time, the state of the FS0B pin and the RSTB pin is high or low.

thank you.

0 Kudos
Reply
3 Replies

2,811 Views
guoweisun
NXP TechSupport
NXP TechSupport

No you can't do that,FS_INIT state can't be skipped.

 

0 Kudos
Reply

2,799 Views
libra_z
Contributor I

thank you for your reply.

According to the connection method in the figure, connect the DBG pin to VBOS through a diode to enter the debug mode. Can FS86 work normally at this time? Does the watchdog need to be refreshed in this mode to skip the INIT_FS state machine?屏幕截图 2022-10-17 100722.png

0 Kudos
Reply

2,662 Views
cuongnguyenvan
NXP Employee
NXP Employee

Hello
A little bit support
(VDBG = VBOS – Vd ≈ 4.5V) Entry the debug mode.
 The DEBUG mode disables the Watchdog, lock FS0B low.
In the InitFSstate, you cannot use the watchdog, and release the safety path pin FS0b.
If you want to use the device, you should switch it to NORMAL_FS where you need to refresh watchdog, exit debug mode, and release FS0b pin

Regards
Cuong

0 Kudos
Reply