FS8500 VPRE Gate Voltage Needed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS8500 VPRE Gate Voltage Needed

3,328 Views
sathishraja17
Contributor I

Hi Team,

We are trying to simulate the VPRE Voltage of PMIC FS8500.

We are in-need of the Gate voltage, Rise/Fall time and duty cycle of High side and Low side of PRE-GHS and PRE-GLS.

The supply is driven through external MOSFET's.

 

Thanks and Regards,

Sathish

0 Kudos
Reply
7 Replies

3,264 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sathish,

please see below an answer from the application team and please find the file mentioned attached.

DESCRIPTION
 

The Rise/Fall time of HS or LS MOSFET is not fixed.

Customer can use attached tool to evaluate the switch time of HS and LS MOSFET. 

They can use the ratio of output and input voltage as the basic value for the duty cycle. And they can consider a dead time about 15-20ns.

JozefKozon_0-1693802717445.png

With Best Regards,

Jozef

0 Kudos
Reply

3,239 Views
sathishraja1
Contributor I

Hi Jozef,

Is there any bootstrap circuitry that is used for driving the gate pin,because there is a pin "PRE_BOOT".

If so kindly do provide details regarding the gate drive circuitry.

 

Thanks,

Sathish

0 Kudos
Reply

3,195 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sathish,

for the connection of the PRE_BOOT pin and for external components used, please refer to the Figure 42. in the FS84/FS85 datasheet and to the KITFS85FRDMEVM schematic. 

JozefKozon_0-1694407931439.pngJozefKozon_1-1694407969469.png

JozefKozon_2-1694408014757.png

With Best Regards,

Jozef

0 Kudos
Reply

3,188 Views
sathishraja1
Contributor I

Hi Jozef,

I meant the Internal Boot strap circuit.PRE-BOOT pin internal circuit.

Does it have any diode to charge the capacitor? and to which supply is it connected..

PFB snapshot from datasheet.

sathishraja1_0-1694410321415.png

Thanks and Regards,

Sathish

0 Kudos
Reply

3,169 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sathish,

another customer had similar question regarding the PRE_BOOT and PRE_SW internal connection. Please see below an answer to him from an application engineer.

DESCRIPTION

PRE_SW is input and monitor source voltage of external High Side FET for internal bootstrap circuit.

JozefKozon_3-1694494548223.png

PRE_SW is a reference internally, to work together with PRE_BOOT.

Then they can generate a high voltage to turn on HS MOS.

So PPRE_SW is just a node for internal circuit.

With Best Regards,

Jozef

0 Kudos
Reply

3,144 Views
sathishraja1
Contributor I
Hi Jozef,
It would be better if it's possible to provide us the high voltage value (internal) to turn on the HS MOS.
Because we are doing a Conducted emission Simulation of the circuit for which we need the approximate gate drive of the internal circuit.

Regards,
Sathish
0 Kudos
Reply

3,109 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sathish,

for the BUK9K52-60E dual MOSFET used on our KITFS85SKTEVM the required Vgs voltage is 5V.

JozefKozon_1-1694602402050.pngJozefKozon_2-1694602418115.png

JozefKozon_3-1694602444782.png

Maximum allowed VGS value is +/-10V.

JozefKozon_4-1694602468460.png

With Best Regards,

Jozef

0 Kudos
Reply