FS8500 VPRE Gate Voltage Needed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FS8500 VPRE Gate Voltage Needed

3,364 次查看
sathishraja17
Contributor I

Hi Team,

We are trying to simulate the VPRE Voltage of PMIC FS8500.

We are in-need of the Gate voltage, Rise/Fall time and duty cycle of High side and Low side of PRE-GHS and PRE-GLS.

The supply is driven through external MOSFET's.

 

Thanks and Regards,

Sathish

0 项奖励
回复
7 回复数

3,300 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sathish,

please see below an answer from the application team and please find the file mentioned attached.

DESCRIPTION
 

The Rise/Fall time of HS or LS MOSFET is not fixed.

Customer can use attached tool to evaluate the switch time of HS and LS MOSFET. 

They can use the ratio of output and input voltage as the basic value for the duty cycle. And they can consider a dead time about 15-20ns.

JozefKozon_0-1693802717445.png

With Best Regards,

Jozef

0 项奖励
回复

3,275 次查看
sathishraja1
Contributor I

Hi Jozef,

Is there any bootstrap circuitry that is used for driving the gate pin,because there is a pin "PRE_BOOT".

If so kindly do provide details regarding the gate drive circuitry.

 

Thanks,

Sathish

0 项奖励
回复

3,231 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sathish,

for the connection of the PRE_BOOT pin and for external components used, please refer to the Figure 42. in the FS84/FS85 datasheet and to the KITFS85FRDMEVM schematic. 

JozefKozon_0-1694407931439.pngJozefKozon_1-1694407969469.png

JozefKozon_2-1694408014757.png

With Best Regards,

Jozef

0 项奖励
回复

3,224 次查看
sathishraja1
Contributor I

Hi Jozef,

I meant the Internal Boot strap circuit.PRE-BOOT pin internal circuit.

Does it have any diode to charge the capacitor? and to which supply is it connected..

PFB snapshot from datasheet.

sathishraja1_0-1694410321415.png

Thanks and Regards,

Sathish

0 项奖励
回复

3,205 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sathish,

another customer had similar question regarding the PRE_BOOT and PRE_SW internal connection. Please see below an answer to him from an application engineer.

DESCRIPTION

PRE_SW is input and monitor source voltage of external High Side FET for internal bootstrap circuit.

JozefKozon_3-1694494548223.png

PRE_SW is a reference internally, to work together with PRE_BOOT.

Then they can generate a high voltage to turn on HS MOS.

So PPRE_SW is just a node for internal circuit.

With Best Regards,

Jozef

0 项奖励
回复

3,180 次查看
sathishraja1
Contributor I
Hi Jozef,
It would be better if it's possible to provide us the high voltage value (internal) to turn on the HS MOS.
Because we are doing a Conducted emission Simulation of the circuit for which we need the approximate gate drive of the internal circuit.

Regards,
Sathish
0 项奖励
回复

3,145 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sathish,

for the BUK9K52-60E dual MOSFET used on our KITFS85SKTEVM the required Vgs voltage is 5V.

JozefKozon_1-1694602402050.pngJozefKozon_2-1694602418115.png

JozefKozon_3-1694602444782.png

Maximum allowed VGS value is +/-10V.

JozefKozon_4-1694602468460.png

With Best Regards,

Jozef

0 项奖励
回复