FS6500 SBC disable Watchdog and RSTB during flashing process

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6500 SBC disable Watchdog and RSTB during flashing process

4,030 Views
fereyes08
Contributor II

I have the following hardware configuration FS6500 and MPC5777C. My application configures the SBC to have INIT_FSSM and INIT_FAULT reaction to trigger FS0B and RSTB as well as the FCCU lines ERROR_0 and ERROR_1 (IO_23) on the SBC side.

My question is: What can I do to disable the SBC watchdog if I want to go to a Programming state (this will jump usually to a bootloader)  to execute ERASE and FLASH process?

Also, is it possible to disable the WD operation at anytime? 

Thanks!

Federico

Labels (2)
Tags (2)
0 Kudos
Reply
3 Replies

3,898 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

If you want to disable the watch dog,please enter into debug mode of SBC.

0 Kudos
Reply

3,898 Views
fereyes08
Contributor II

Hello,

Thanks for your reply. Unfortunately DEBG mode requires a HW line to be pulled and a POR. In our application we are in RUN mode and at some point of time either for flashing purposes or after run (prepare the ECU to sleep) we want to disable the Q&A or the RESET of the FS6500.

Thanks!

0 Kudos
Reply

3,898 Views
guoweisun
NXP TechSupport
NXP TechSupport

Understand your question,but I am afraid that is difficult to control disable watchdog during the system active.

0 Kudos
Reply